Keysight Oscilloscope Overview
The 89600 VSA software supports the following Keysight Oscilloscopes:
There are several factors to consider in using oscilloscopes as the Measurement Hardware:
- Analog bandwidth can affect the signal by slowing the rise time and by attenuating the amplitude. It is important to determine the required analog bandwidth for your particular application.
- The Sampling technique used depends on the type of signal (repetitive or not). For Real Time sampling, the best resolution between points is the inverse of the sample rate.
- Deep memory options are available in some oscilloscopes. Deeper memory enables longer periods of time to be captured while maintaining a high sample rate.
- Oscilloscopes can offer multiple channel measurements. The 89600 VSA software can make up to 4 channel measurements with selected scopes.