Sidelobe Keep Out Mode (Pulse)

Menu Path: Analysis > Pulse Properties > Correlation

Sidelobe Keep Out Mode selects between first null or a minimum time criteria to distinguish the sidelobe from the main lobe.

First Null searches for the first null point outside from the main lobe then sets the region between the points as keep out time. Enable Correlation/Sidelobe Calculations must be selected to make this setting available.

Time specifies the keep out time as defined in the Sidelobe Keep Out Time parameter.

Default: First Null

Choices: First Null, Time

See Also

Enabling Time Sidelobe/Correlation Calculations

Pulse Table