Sidelobe Keep Out Time (Pulse)

Menu Path: Analysis > Pulse Properties > Analysis > Correlation

Sidelobe Keep Out Time If a time criterion was selected for the keep out mode, then the user may specify a minimum correlation time away from the main lobe to start looking for the peak correlation of the sidelobe. Without some minimum time, the sidelobe could be easily confused with the main lobe. Keep-out time is the time around the main lobe that is ignored when searching for sidelobes.

Enable Correlation/Sidelobe Calculations must be selected to make this setting available.

Default: 0.0

See Also

Enabling Time Sidelobe/Correlation Calculations

Pulse Table