Sidelobe Minimum Rho (Pulse)

Menu Path: Analysis > Pulse Properties > Analysis > Correlation

Sidelobe Minimum Rho sets the minimum similarity index (Rho) for time sidelobe calculations. For each pulse, time sidelobe calculations are done only if the Rho value for that pulse is greater than or equal to this value. Enable Correlation/Sidelobe Calculations must be selected to make this setting available.

Default: 0.5

Choices: 0 - 1 (unitless)

See Also

Enabling Time Sidelobe/Correlation Calculations

Pulse Table