Sidelobe Search Range Ratio (Pulse)

Menu Path: Analysis > Pulse Properties > Analysis > Correlation

Sidelobe Search Range Ratio sets an upper bound to the time search range for time sidelobe calculations, as a percent of the pulse width. Enable Correlation/Sidelobe Calculations must be selected to make this setting available.

Default: 200%

Range: 0 - 500%

See Also

Enabling Time Sidelobe/Correlation Calculations

Pulse Table