Scoring Metric
Menu Path:
The Scoring value is a calculated index of overall pulse quality by comparing pulse parameters/metrics (Top Level, Width, PRI, Freq Mean and FM Frequency Modulation Slope) with the reference pulse(s) relative to base error values (Top Level, Width, PRI, Freq Mean and FM Slope) set in the Scoring tab. The scoring index is calculated using the following formula:
where
represents the score,
is the number of scoring metrics,
is the measured value,
is the reference value, and
is the base error of the
-th metric.
The Scoring metric's column visibility is disabled by default. To enable the Scoring column, right-click the header for any column in the Table and check the Scoring checkbox. See Column Visibility for details.