Pulse Demod Bits
Menu Path:
The Pulse Demod Bits trace is available for long demodulation when BPSK and/or QPSK Pulse Modulation types are selected and Enable extended bits (BPSK/QPSK)is enabled.
The Pulse Demod Bits trace is split into two halves: the top showing Pulse Number (the pulse selected by Starting Pulse), Modulation Type and Length (chips); the bottom showing the demodulated bits in binary format.
You can assign a marker to the Pulse Bits trace to navigate the demodulated bits using the arrow keys. The marker's X unit is always per chip.
See Also