Result Tables (Pulse)
Menu Path:
The Pulse Measurement allows you to display tables that list reported performance metrics for each detected pulse within the current acquisition. See the Matrix Tables reference topic for more information.
You can select from the following table formats.
-
Pulse Table – displays list of reported performance metric for each detected pulse within current Acquisition Time interval.
-
Pulse Train Search Table – displays pulse train search and scoring results when Pulse Train Scoring is selected and enabled in the Analysis > Scoring panel.
-
Cumulative Pulse Table – displays accumulated list of reported performance metric for each detected pulse since last Measurement Restart event (includes current plus previous acquisitions). Any pulse without complete data is considered incomplete and not included in the calculations.
-
Cumulative Statistics – displays accumulated statistics of each reported performance metric based on all detected pulse since last Measurement Restart event (includes current plus previous acquisitions). Any pulse without complete data is considered incomplete and not included in the calculations.
-
Current Statistics – displays Min Max, Avg, Std Dev of each reported performance metric based on set of detected pulses within current Acquisition Time interval.
-
Demod Bits - displays demodulated bits in binary format when Enable extended bits (BPSK Binary phase shift keying - A type of phase modulation using 2 distinct carrier phases to signal ones and zeros./QPSK Quadrature phase shift keying) is enabled.
-
Summary - display Average Power, Peak Power, Detection Threshold, Top Level, Base Level, Top/Base and Time Offset for the current acquisition.
See Also