CDF (6GR)
The trace shows the cumulative distribution function (CDF Cumulative Distribution Function: The cumulative probability that a parameter will be less than a given value X.) of the selected input channel. The CDF is computed by integrating the PDF (probability density function), and is described further in the CCDF topic.
The CDF is computed from the data in the Time trace.
See Also