Time (6GR)
The trace is the time-corrected portion of the Search Time data that is used for the measurement analysis.
The Analysis Start Boundary, Subframe Offset, and Subframe Interval parameters determine which portion of the Result Length is included in the trace.
See Also