PDF (6GR)
The trace shows the probability density function (PDF 1) Probability Density Function Trace Data, or 2) Portable Document Format (PDF) created by Adobe Systems is an open standard for document exchange.) of the selected input channel. The PDF indicates the probability that a given signal level has occurred.
The PDF is computed from the data in the Time trace.
For a more detailed description of this trace, see PDF trace data in the Reference.
See Also