Eq Condition Number (6GR)
The traces in the CCn and Selected Display CC menus are identical and show the same CC0 information.
The trace shows the MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. channel's condition number — the ratio of the maximum to minimum singular value of the channel matrix — versus frequency. The condition number is a measure of how well-conditioned (separable) the spatial channel is; higher values mean the streams are harder to separate.
This result is computed only when multiple data streams are present; for a single-stream signal it has no meaningful value. The computation is configured by and on the EVM section of the Advanced tab.
See Also