Raw Main Time (6GR)
The trace shows the raw time data read from the input hardware or playback file for the selected channel. Resampling and time adjustment are performed on and the result is shown in the Search Time trace.
Characteristics of this trace:
- The data has not had instrument calibration corrections applied, so the trace shows a "CAL?" trace message.
- The data has not gone through the analyzer's software resampling filters, so it is generally not sampled at the specified sample rate.
- The zero time point is where the instrument or the recording actually triggered.
See Also