Search Time (6GR)

The Search Time trace shows the time record data after resampling and time adjustment have been applied to the Raw Main Time data. This is the data the demodulator searches to synchronize with the signal.

The 6GR demodulator uses an internal synchronization algorithm, so there is no separate search time length parameter. The amount of data acquired is set by Result Length and Acquisition Mode, and the portion of it that is analyzed — and therefore shown in the Time trace — is set by Analysis Start Boundary, Subframe Offset, and Subframe Interval.

See Also

Raw Main Time

Time

Time Parameters

Available Trace Data