Normalize IQ Traces (RFID)
: Selected (See RFID Standard Setups/Presets Table)
Selecting the check box turns on normalization; clearing the check box turns off normalization.
Normalization is always applied to most ASK and OOK modulation measurements regardless of the setting of the check box.
ASK Meas Time with CW is not normalized.
When normalization is on, the VSA normalizes or scales the demodulated trace data results to a nominal value of 1. Normalization is performed on these traces:
- FSK Frequency Shift Keying: A form of modulation using multiple carrier frequencies to carry the digital information. The most common is the two frequency FSK system using the two frequencies to carry the binary ones and zeros. measured time (FSK measurements)
- FSK measured reference (FSK measurements)
- FSK error (FSK measurements)
How Normalization Works with ASK
For ASK, normalization scales the demodulated data as follows:
|
ASK Trace |
Scaling |
|---|---|
|
ASK Measured Time |
Deviation |
|
ASK Reference Time |
Deviation |
|
Carrier Magnitude Error |
rms magnitude |
|
ASK Error Time |
Deviation |
How Normalization Affects the Trace Measurement Units
For most configurations, the measurement data determines the units of the normalized trace. With normalization on, the y-axis units (for rectangular traces) or polar units (for polar traces) become unitless or are converted to a percentage. If the trace format is selected, the units are decibels.
See Also
IQ Normalize (Digital Demodulation)
Advanced Tab (RFID Demod Properties)