Meas Time With CW (RFID)
The Demod trace displays the demodulated signal trace that has been filtered, resampled and frequency, phase compensated. The default display format of this trace is Linear Mag.
When modulation format is SSB-ASK, the signal frequency is compensated using the CW tone that precedes and follows the SSB signal; and phase compensation is not done.
The trace title is determined by the type of modulation format specified by the Fwd Format or the Ret Format selected on the Format Tab (RFID). When the modulation format specified is , the trace title will read and when the modulation format is specified as , the trace title will read .
This trace is not available for FSK Frequency Shift Keying: A form of modulation using multiple carrier frequencies to carry the digital information. The most common is the two frequency FSK system using the two frequencies to carry the binary ones and zeros. measurements.
See Also