Using Standard Setups and Presets
There are two ways to configure the VSA for RFID demodulation measurements: manually specify the demodulator protocol configuration parameters or select a preset standard format for your RFID system and the VSA will automatically set the protocol configuration parameters. Note that in some standards formats, the line coding will vary depending on the bit rate used.
The following list shows the standard protocol presets supported by the VSA. Entries followed by the notation "Beta" are preliminary releases. Click on the standard link to view the default parameter settings.
| Available Standard Presets |
|---|
|
ISO 18000-4 Mode-1 (Beta) |
|
ISO 18000-6 Type-A (Beta) |
|
ISO 18000-6 Type-B (Beta) |
Available "Preset to Standard" Protocols
|
Tab |
Parameter |
FWD Value |
RET Value |
|---|---|---|---|
|
Format |
Format |
DSB-ASK |
DSB-ASK |
|
|
Line Coding |
PIE-C |
FM0 |
|
|
Measurement Mode |
MOD Analysis |
MOD Analysis |
|
|
Auto Bit Rate/Tari |
ON |
ON |
|
|
Bit Rate |
160kbps |
40 kbps |
|
|
Tari |
6.25μs |
--- |
|
|
Points/Symbol |
20 |
20 |
|
|
Span |
6.4MHz |
6.4MHz |
|
|
|
|
|
|
Filter |
Meas Filter |
None |
None |
|
|
Ref Filter |
None |
None |
|
|
Alpha |
0.5 |
0.5 |
|
|
|
|
|
|
Time |
Acquisition Length |
10ms |
10ms |
|
|
Burst Search |
ON |
ON |
|
|
Burst Index |
0 |
0 |
|
|
Result Length |
1ms |
1ms |
|
|
Result Offset |
0s |
0s |
|
|
Sync Search Length |
1ms |
1ms |
|
|
Sync Search Offset |
0s |
0s |
|
|
|
|
|
|
Sync Search |
Sync Search |
OFF |
OFF |
|
|
Sync Search Type |
Standard |
Standard |
|
|
Standard Sync Pattern |
EPCGlobal C-1Gen-2 FWD Preamble |
EPCGlobal C-1Gen-2 RET FM0 TRext0 |
|
|
|
|
|
|
Advanced |
IQ Normalize |
ON |
ON |
|
|
Mirror Frequency Spectrum |
OFF |
OFF |
|
|
CW Lower |
10% |
10% |
|
|
CW Upper |
90% |
90% |
|
|
ASK Lower |
10% |
10% |
|
|
ASK Upper |
90% |
90% |
|
|
CW Settling |
5% |
5% |
Return to the Available Presets Table.
Return to the Available Presets Table.
Return to the Available Presets Table.
Return to the Available Presets Table.
Return to the Available Presets Table.
Return to the Available Presets Table.
Return to the Available Presets Table.
See Also
RFID Demod Properties Dialog Box