Measurement Filter (RFID)
None (See RFID Standard Setups/Presets Table)
The dropdown list selects the measurement filter. This filter is applied to the measured data before synchronization and demodulation. The available selections are:
- None
- Root Raised Cosine
Though filtering is not defined in the RFID standards, the signal is often shaped by some type of filter, so it is often worthwhile to have a and . The value of the filter is specified by the value entered in the box.
Filtering can cause problems with tari- or bit rate-based searches.
See Also
Filter Tab (RFID Demod Properties)