Reference Filter (RFID)
None (See RFID Standard Setups/Presets Table)
The dropdown list selects the reference filter. The available selections are:
- None
- Raised Cosine
- Gaussian
Though filtering is not defined in the RFID standards, the signal is often shaped by some type of filter, so it is often worthwhile to have a Reference filter.
The Alpha or BT Bandwidth Time Product parameter of the filter is specified by the value entered in the box.
See Also