Preset to Standard (RFID)
EPC Global Class-1 Generation-2 UFH (ISO 18000-6 Type-C) (See RFID Standard Setups/Presets Table)
EPC Global Class-1 Generation-2
UFH (ISO 18000-6 Type-C)
ISO 18000-4 Mode-1 (Beta)
ISO 18000-6 Type-A (Beta)
ISO 18000-6 Type-B (Beta)
ISO 18092
ISO 14443 Type-A
ISO 14443 Type-B
ISO 15693
To see a listing of the settings for each of these protocols, see Using Standard Setups/Presets.
After selecting the RFID demodulator, specify a specific RFID protocol. The demodulator protocol configuration parameters can be manually specified or a standard setup can be selected and then the settings modified to your needs. The button configures the RFID demodulation software to one of several settings designed to properly demodulate a specific RFID protocol.
See Also