Format Tab (RFID)
The tab of the selects the RFID protocol, Direction, Format, Line Coding, Measurement Mode, Bit Rate, Tari, and Points/Symbol. These controls allow easy specification of the RFID signal to be examined and the major parameters of that signal.
The Format tab configures these parameters:
- Measurement Mode
- Preset to Standard
- ASK Auto Bit Rate / Tari
- Direction
- Fwd
- Ret
- Points / Symbol
- Passive Return link
See Also
Filter Tab (RFID Dempd Properties)
Time Tab (RFID Dempd Properties)
Sync Search Tab (RFID Dempd Properties)
Advanced Tab (RFID Dempd Properties)
RFID Demod Properties Dialog Box