Burst Summary (RFID)
is a summary table of the characteristics of the signal Burst. The default display format of this trace is Real.
The table has 5 columns providing the following information:
- # is the position of the burst in the CW signal. Bursts are numbered starting at zero.
- is the time between the beginning of the acquisition time and the beginning of the burst.
- is the length of the burst.
- (forward or return) is the direction of the burst.
- the interval between bursts preceding the numbered burst. For burst #0, the table displays "---" for the Off Interval value because there is no preceding burst.
Fifteen bursts are displayed. The Burst Index determines the burst is centered around. For example, if the Burst Index is 15, the table will show burst # 8 - 22.
Refer to the following diagram.
See Also