Burst Index (RFID)
0 (See RFID Standard Setups/Presets Table)
0 to 99
specifies the burst to demodulate and measure.
This parameter is available only when is .
The offset and length of each burst included in the acquired signal are recognized by a algorithm. However, modulation quality results are computed from only one burst, which is specified by the . The offset and length of the burst specified by is used to determine the result offset and result length for the measurement.
The Acquisition Time trace uses background shading to show the bursts that have been found. The background shading and highlighting will show the number.
The Burst Summary Table displays the characteristics of the signal bursts. Fifteen bursts are shown at a time. The Burst Index determines the burst the table is centered around. For example, if the Burst Index is 15, the table will show burst # 8 - 22.
See Also
Sync Search Tab (RFID Demod Properties)