Burst Search (RFID)
On (See RFID Standard Setups/Presets Table)
On or Off
When is selected, the offset and length of each burst included in the acquired signal are recognized by a algorithm. However, modulation quality results are computed from only one burst, which is specified by the . The offset and length of the burst specified by is used to determine the result offset and result length for the measurement.
If the last burst in the Acquisition Time is a forward burst, the burst search will sometimes misidentify noise after the forward burst as a return burst.
If the last burst in the Acquisition Time is a return-link burst and the burst ends very close to the end of Acquisition Time or extends past the end of Acquisition Time, then the burst search may erroneously indicate that the burst ends earlier than it really does. To work around this, ensure that the return-link burst ends well before the end of Acquisition Time.
When is selected for the is the same as and the determines the measurement region.
The following diagram shows how sync-related parameters are used when Burst Search is :
When is set to , The , , , , and are specified by entering values in the entry boxes in the area of thetab.
The following diagram shows how sync-related parameters are used when Burst Search is :
A message can indicate that the beginning or end of a burst is too close to the edge of the acquisition record for the software to determine the proper sync. To correct this problem, increase the acquisition length or increase the trigger delay to move the CW envelope edges away from the start or end of the acquisition time.
See Also