Fall Time (RFID)
Menu Path:
Fall Time is calculated as microseconds from Demod . The Avg min and max are calculated for a single scan. See the following illustration.
See Also
Menu Path:
Fall Time is calculated as microseconds from Demod . The Avg min and max are calculated for a single scan. See the following illustration.
See Also
|
Copyright © 2000-2026 Keysight Technologies, Inc. |