Demod Summary (RFID)
The table displays the results of the RFID demodulation analysis. The information presented in the trace table depends on the type of modulation format specified by the Fwd Format or the Ret Format selection on the Format tab and on the direction of the burst specified by the Burst Search parameters. The table types are:
Generating the Table Data
The RFID demodulation analysis generates two traces, and . (is created by removing CW from the trace.)
These two Meas Time traces are normalized by
, where:
,
,
Ai : On-Amplitude of i-th pulse,
Bi : Off-Amplitude of i-th pulse,
N : Number of pulses.
Therefore, all amplitude-related results are calculated from these two
traces are normalized by
.
The average Mod Depth is defined as:
.
The average Mod
Index is defined as:
.
The following illustration shows how RFID derives some measurements.
The table below describes the ASK Summary Table entries:
| ASK Summary Table Entries | ||
|---|---|---|
See Also