LocalMaxTime (RFID)
Menu Path:
LocalMaxTime is defined in the ISO 18092 and ISO 14443 Type A standards. The Summary NFC Table (RFID) shows the average, maximum, and minimum values of this value.
LocalMaxTime is the time between a local maximum and the time of passing the same value before the local maximum, computed over the “fall time” part of each pulse. Refer to the illustration below. If there is more than one local maximum within a single fall time, only the largest is used.
LocalMaxTime is calculated from Demod . The average, maximum, and minimum values are calculated for a single scan.
See Also