Summary NFC Table (RFID)
The table displays the results of the RFID analysis for signal parameters defined for Near Field Communications (NFC).
The following illustration shows how RFID derives measurements:
t2 off time starts from the last time the signal falls below the lower threshold (5%).
The table below describes the table entries:
Summary NFC Table Entries
See Also