Bits (RFID)
Menu Path:
The Demod trace displays the demodulated bits of the burst highlighted in the trace after they have been decoded using the selected .
The possible characters in this table are as follows:
- 0 or 1 - data bits
- x - invalid data
- S - start of frame
- E - end of frame
- D - delimiter
- R - RTCal symbol
- T - TRCal symbol
See Also