Fwd Line Coding (RFID)
: PIE(EPC C1 Gen2) (See RFID Standard Setups/Presets Table)
selects the line coding expected by the RFID demodulation software. This value is preset when a protocol is selected using the button. To provide flexibility, the line coding value can be independently set.
The dropdown list selects the format of the RFID modulation. The available values are:
- None (NRZ Non Return to Zero)
- Manchester
- FM0
- PIE (ISO 18000-6 Type A)
- PIE (EPC C1Gen2)
- Modified Miller
- 1 out of 4
- 1 out of 256
When is selected as the RFID standard and is set to either or , is set as follows:
- : Fwd Bit Rate set to 26.484375 kbps
- : Fwd Bit Rate set to 1.6552734375 kbps
See Also
Format Tab (RFID Demod Properties)