Ret Line Coding (RFID)
FM0 (See RFID Standard Setups/Presets Table)
The dropdown list selects the format of the RFID modulation. The available values are:
- None (NRZ Non Return to Zero)
- Manchester
- FM0
- Miller
- Miller-2
- Miller-4
- Miller-8
- Modified Miller
- Subcarrier Manchester
- 15693 Single Subcarrier Manchester Low Rate
- 15693 Dual Subcarrier Manchester Low Rate
- 15693 Single Subcarrier Manchester High Rate
- 15693 Dual Subcarrier Manchester High Rate
- Subcarrier BPSK Binary phase shift keying - A type of phase modulation using 2 distinct carrier phases to signal ones and zeros. 1
- Subcarrier BPSK 2
- Subcarrier BPSK 4
- Subcarrier BPSK 8
The dropdown list selects the line coding expected by the RFID demodulation software from the Tag. This value is preset when a protocol is selected using the button. To provide flexibility, the line coding value can be set independently.
See Also