Result Length (RFID)
1 mSec (See RFID Standard Setups/Presets Table)
0 to (cleared)
0 to (selected)
The text box is active when is cleared.
The text box sets measurement interval in seconds. (Since it is difficult to specify measurement interval using Bits or Tari when PIE is selected in ASK mode, the units are in seconds.)
See Also
Time Tab (RFID Demod Properties)