RFID Demod Properties Dialog Box

The RFID (Radio Frequency Identification) Demod dialog box contains parameters that configure the VSA to demodulate RFID modulated signals.

RFID demodulation must be selected before this dialog box is available. To enable RFID demodulation, click Analysis > Type > Other standard formats > RFID.

The RFID Demod Properties Dialog Box contains the following tabs:

See Also

Selecting the RFID Demodulator

Setting Up an RFID Measurement

Using Standard Setups (RFID)