Spread Code Length CDP Layer (TD-SCDMA)
16 (80 ksyms/s) (See TD-SCDMA Standard Setups/Presets Table.)
: 1, 2, 4, 8, or 16
CDP Layer selects the active code domain layer () for the CDP Layer trace data. This parameter has no other effect except for the display of the and trace data.
Selecting a CDP Layer Spread Code Length
Click one of the available TD-SCDMA from the drop-down list.
The marker does not automatically specify the CDP Layer .
See Also