Max Users (K) (TD-SCDMA)
16 (See TD-SCDMA Standard Setups/Presets Table.)
:2, 4, 6, 8, 10, 12, 14, 16
specifies the number of Maximum Users (K) that will be associated with the timeslots specified by the Traffic TimeSlots parameters.
Use in the parameter selection to associate all timeslots with the specified value.
See Also