Preset to Standard (TD-SCDMA)
configures the demodulator to analyze a 3GPP N-TDD Time Division Duplex: A duplexing technique dividing a radio channel in time to allow downlink operation during part of the frame period and uplink operation in the remainder of the frame period. 1.28Mcps, TD SCDMA modulated signal. See Using a TD-SCDMA Standard Setup for more information.
See Also
Format Tab (TD-SCDMA Demod Properties)
Using a TD-SCDMA Standard Setup
Selecting TD-SCDMA Demodulation