Measurement Speed Considerations (TD-SCDMA)
The primary factor in the measurement speed for TD-SCDMA measurements is the amount of input data that must be processed. Reducing the result length is the best way to increase speed.
See Also
Setting Up a TD-SCDMA Measurement