Troubleshooting (TD-SCDMA)
This topic contains information to help you troubleshoot measurements when using TD-SCDMA Demodulation. You should also review Setting up a TD-SCDMA Measurement for additional measurement information.
|
PROBLEM |
POSSIBLE CAUSE |
SOLUTION |
|---|---|---|
|
Demodulation fails to lock-on to signal |
Signal not present |
Check test setup connections |
|
|
Carrier too far from center frequency |
Adjust center frequency to ± 500 Hz of the carrier frequency |
|
|
|
|
|
|
Input signal is over-loaded or under ranged |
Adjust input range |
|
|
|
|
|
|
Frequency span is too narrow |
Increase frequency span |
|
|
|
|
|
|
Incorrect Chip Rate |
Enter the correct chip fate (not symbol or bit rate) |
|
|
|
|
|
|
No Pilot Channel: missing or level too low |
Set pilot channel at Walsh Code Number Zero. Try adjusting pilot channel power level. |
|
|
|
|
|
|
TD-SCDMA signal spectrum is inverted |
Check the Mirror Frequency Spectrum setting (Analysis > TD-SCDMA Demod Properties > Advanced tab). |
|
|
|
|
|
|
I/Q Offset too large |
Reduce the LO feedthrough (or DC Offset for I+jQ receiver) |
|
|
|
|
|
Wrong channel marked as active |
Poor SNR Signal-to-Noise Ratio (signal to noise ratio). |
Increase signal power or remove cause of noise/distortion. |
|
|
|
|
|
|
All bits not transmitted within a physical channel. |
Transmit all bits within a physical channel, or select code-domain power for the layer associated with the physical channel of interest (single-layer code-domain power displays are accurate even if the VSA is unable to identify active channels in the composite code-domain power display). |
|
|
|
|
|
|
Data pattern induces large disparity in power between slower channels overlaid by the channel of interest. |
Verify that your transmitter is transmitting properly. |
|
|
|
|
|
ADS application has failed to work with TD-SCDMA demodulation |
|
|
|
The trace data constellation symbol location shape, such as dots, is not properly displayed. |
The display driver is not functioning correctly. |
Contact your PC manufacturer to see if a newer version of the display driver is available. If not, try decreasing the hardware acceleration. See the Windows documentation for instructions. |
See Also
Setting Up a TD-SCDMA Measurement
Measurement Speed C considerations