Left / Right DataPwr (TD-SCDMA)  

Left DataPwr (Left Data Field Power) provides the absolute power measurement (in dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer) for the data segment before the preamble for each timeslot within the analyzed sub-frame.

Right DataPwr (Right Data Field Power) provides the absolute power measurement (in dBm) for the data segment after the preamble for each timeslot within the analyzed sub-frame. This includes power data results for sub-frame timeslots 0 through 6. The 3GPP standard requires separate power normalization for data segments before and after the preamble.

The data results are for the analyzed sub-frame, which is specified in the Analysis Sub-frame parameter list box (Analysis > TD-SCDMA Demod Properties > Time tab > Analysis Sub-frame).

See Also

Available Overall Error Summary Data

Overall Error Summary Data