TotPwr (TD-SCDMA)  

The Overall Error Summary table provides the absolute power measurement (in dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer) for:

The data results are for the analyzed sub-frame, which is specified in the Analysis Sub-frame parameter list box (Analysis > TD-SCCMA Demod Properties > Time tab > Analysis Sub-frame).

See Also

Available Overall Error Summary Data

Overall Error Summary Data