Pilot Tracking (TEDS)
Selected (See Using Standard Setups/Presets)
Includes pilot tracking in Error Vector Magnitude (EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format.) calculations and adjusts constellation diagrams.
, when selected, causes the VSA to analyze the predicted locations of the pilot symbols on the sync/pilot locus versus the actual pilot symbol locations and add phase/amplitude corrections to better position the actual pilot symbols at the predicted locations. You can view this feature visually by displaying a subcarrier constellation trace and then selecting and clearing the parameter. Similarly, display an EVM calculation, and then select and clear the parameter to see the effects of pilot error on the EVM calculation.
See Also