Slot Offset (TEDS)
0
0 to Contiguous Slots - 1
specifies which slot within the set of contiguous active slots will be used for modulation analysis. Setting this value to zero implies the first slot of the set of contiguous slots will be analyzed.
The and parameters are only available when Slot Format is set to or . For other slot formats, the and parameters are disabled and have no effect on analysis.
See Also