Contiguous Slots (TEDS)
1
1 to number of slots possibly contained in Search Length
specifies how many slots are assumed to be contiguous in an uplink slot. This setting configures the RF Radio Frequency: A generic term for radio-based technologies, operating between the Low Frequency range (30k Hz) and the Extra High Frequency range (300 GHz). envelope search algorithm to provide detection of the start of a series of contiguous slots.
The and parameters are only available when Slot Format is set to or . For other slot formats, the and parameters are disabled and have no effect on analysis.
See Also