Slot Format (TEDS)
See Using Standard Setups/Presets
allows you to select one of the following TEDS slot formats:
- - 14.167 ms
- - 14.167 ms
- - 7.083 ms
- - 7.083 ms
Another method for selecting the slot format is to use the button which prompts you to select a slot format. The Channel Bandwidth must be set prior to using the button. Then sets up the parameters for the selected channel bandwidth. (See Using Standard Setups/Presets.)
See Also