Resolution Bandwidth (TEDS)

Resolution Bandwidth (ResBW) in the VSA is entirely dependent on the Window Type chosen and the length of time being analyzed. In a TEDS measurement, the length of time being analyzed cannot be set. It is the length of the timeslot being analyzed. Thus the Resolution Bandwidth on the Analysis > Frequency > ResBW tab is dimmed and entries by double-clicking ResBW on the Spectrum trace are ignored. The only trace to which Resolution Bandwidth pertains is the Spectrum trace so that is why changing the Window Type only affects the Spectrum trace.

See Also

TEDS Demod Overview

Typical TEDS Measurements