Overlaid IQ Mag Error (TEDS)

Overlaid IQ Mag Error shows IQ magnitude error for all the TEDS subcarriers corresponding to your Channel Bandwidth setting, on a symbol-by-symbol basis. Each colored vertical line represents a symbol. The number of symbols is determined by the slot format selected. These lines are overlaid with a white trace that shows the average IQ magnitude error per symbol (LinMag scale only). The trace below is a Normal Uplink, 50kHz channel bandwidth, 16QAM modulation signal. The 31 colored vertical lines (0 to 30) represent the 31 symbols in a Normal Uplink slot format. Each line contains points from the 16 subcarriers corresponding to the 50kHz channel bandwidth. See TEDS Subcarriers for more information on the number of subcarriers for each channel bandwidth.

Select Trace > Auto Scale to scale the trace. If the trace shows NO DATA, check your recorded signal or hardware input and TEDS demod properties. TEDS demod parameters Droop and Pilot Tracking affect this trace. The above trace shows a LinMag (linear magnitude) scale. To change scales, see Trace > Format and choose from the  format drop-down menu.

Select Marker > Show Marker to place a marker on the trace; then review the symbol information in the marker readout window. Once you have a marker on the trace, use your up, down, left, and right arrow keyboard keys to move the marker through the symbol points.

IQ magnitude error refers to the difference in the measured magnitude for an IQ phasor versus the magnitude of the ideal (reference) phasor.

To view IQ magnitude error for a specified subcarrier, see IQ Mag Error (Ch1 Subcarr).

See Also

About TEDS Trace Data