External Reference Lock Status Messages
These messages, which appear at the bottom of the window, indicate the status of the external reference.

|
Message |
Explanation |
|---|---|
|
|
External reference status message. The 89600 VSA uses the reference signal generated internally by the input module. |
|
|
External reference status message. The 89600 VSA is locked to a signal at the external reference connector. |
|
|
External reference status message. The 89600 VSA is locked to the clock signal provided by the reference instrument. |
|
|
External reference status message. The Lock Reference state for a piece of hardware that is used in conjunction with other hardware modules has been changed from True to False. Or the external reference for a piece of hardware that has Lock Reference set to True could not lock to the external reference. |
See also