Active Channel Threshold (W-CDMA(3GPP)/HSPA)
Auto (See W-CDMA(3GPP) Standard Setups/Presets Table.)
allows toggling the active Code Channel detection threshold level between and modes.
|
: |
The internal algorithm determines the active code channel identification automatically. |
|
: |
The active code channel identification is determined by the setting. |
The provides a method to improve the automatic active code channel detection algorithm. Manual override is required for signals that cause incorrect active code channel identification which will lead to incorrect composite data results.
See Also