Dialog Box and Tabs (W-CDMA(3GPP)/HSPA)

The W-CDMA Code Division Multiple Access: One of several digital wireless transmission methods in which signals are encoded using a specific pseudo-random sequence, or code, to define a communication channel. A receiver, knowing the code, can use it to decode the received signal in the presence of other signals in the channel. This is one of several "spread spectrum" techniques, which allows multiple users to share the same radio frequency spectrum by assigning each active user an unique code. CDMA offers improved spectral efficiency over analog transmission in that it allows for greater frequency reuse. Other characteristics of CDMA systems reduce dropped calls, increase battery life and offer more secure transmission. See also IS-95. (3GPP)/HSPA Demod Properties dialog box contains properties and parameters that to configure the VSA to descramble, despread, and demodulate W-CDMA (3GPP) and HSPA standard signals.

The W-CDMA(3GPP) demodulator must be selected before this dialog box is available. To enable the demodulator, click Analysis > Type > Cellular > W-CDMA (3GPP)/HSPA.

The W-CDMA (3GPP)/HSPA Demod Properties dialog box contains tab headings that group similar configuration parameters as follows:

See Also

Selecting W-CDMA(3GPP) demodulator

Setting up a W-CDMA(3GPP) Measurement

Troubleshooting W-CDMA(3GPP)