Use Multichannel Estimator
Clear (SeeW-CDMA(3GPP) Standard Setups/Presets Table.)
excludes or includes the active Code Channel Timing offset and Phase offset data results in the CDP Code Domain Offsets trace results. The measurement speed is much faster when the Timing offset and Phase offset data results are excluded from the measurement. If those data results are not required, it is recommended to exclude them in the computed CDP Code Domain Offsets trace data.
(default): The Code Domain Power Timing Offset and Phase Offset error data results are not computed and are removed from the error results from the CDP Code Domain Offsets trace data results.
: The Code Domain Power Timing Offset and Phase Offset error data results are included the CDP Code Domain Offsets trace data results.
See Also
Advanced Tab - W-CDMA(3GPP)/HSPA Demod Properties
W-CDMA(3GPP)/HSPA Demod Properties